Section
Author's Guide | Reviewer's Guide

ST Journal of Research
Index (Vol. 3, No. 1)

MEMS
 
MEMS applications

MEMS: The secret revolution

Today the Semiconductor Industry has reached the astonishing value of $250 B. And even more surprisingly, it all started from a simple silicon transistor, which replaced mature and reliable vacuum tubes thanks to its semiconductor properties. Lithography has been the driving force of this industry according to Moore’s Law.

But in the same decades and in the same manufacturing plants a few pioneers have been exploiting other physical properties of silicon without following the path of submicron technologies and 12” wafer fabs. And all those explorers, outside of the mainstream technology development roadmap highlighted and supported by the Semiconductor Industry Association, have faced many theoretical and practical challenges to bring their ideas to the market. (More...)

 
Vol. 3, No. 1, August 2006 - Table of Contents
Art. 1 More than Moore: micro-machined products enable new applications and open new markets by B. Vigna (STMicroelectronics) p. 4
Art. 2 Out of plane vs. in plane flexural behaviour of thin polysilicon films:
mechanical characterization and application of the Weibull approach
by F. Cacchione, A. Corigliano - Politecnico di Milano, B. De Masi, C. Riva - STMicroelectronics p. 15
Art. 3 A capacitance and optical method for the static and dynamic characterization of MEMS devices by Eleonora Ferraris, Irene Fassi, Institute of Industrial Technology and Automation, Biagio De Masi, STMicroelectronics, Richard Rosing, Andrew Richardson, Lancaster University p. 21
Art. 4 Novel process for realization of multiple axis actuators suitable for the realization of an optical switch by Marco Del Sarto, Simone Sassolini, Mauro Marchi, Lorenzo Baldo, STMicroelectronics p. 29
Art. 5 Electrostatic analysis of a comb-finger actuator with Schwarz–Christoffel conformal mapping by P. Bruschi, A. Nannini, F. Pieri, G. by Raffa, University of Pisa, B. Vigna, S. Zerbini, STMicroelectronics p. 38
Art. 6 Control of a Z-Axis MEMS Vibrational Gyroscope by Roberto Oboe, Member, IEEE, Riccardo Antonello, Student Member, IEEE, Ernesto Lasalandra, Guido Spinola Durante, and Luciano Prandi, STMicroelectronics p. 53
Art. 7 Optical Detection of the Coriolis Force on a Silicon Micromachined Gyroscope by Valerio Annovazzi-Lodi, Sabina Merlo, Michele Norgia - University of Pavia, Guido Spinola, Benedetto Vigna, and Sarah Zerbini- STMicroelectronics p. 63
Art. 8 An Above IC MEMS RF Switch by Daniel Saias, Philippe Robert, Samuel Boret, Christophe Billard, Guillaume Bouche, Didier Belot, and Pascal Ancey, STMicroelectronics p. 74
Art. 9 A simple lumped electrical model for an RF MEMS switch considering lossy substrate effects by Giuseppe Cusmai, Marco Mazzini, Paolo Rossi, Francesco Svelto, University of Pavia; Chantal Combi, Benedetto Vigna, STMicroelectronics p. 83
 

Download Full Issue (PDF Format) Size 7 MB