Section
 

Product Range 

STMicroelectronics produces one of the industry’s broadest ranges of semiconductor products, from discrete diodes and transistors through complex System-on-Chip (SoC) devices to complete platform solutions that bundle chips with reference designs, application software, and manufacturing tools and specifications. With particular strengths in digital multimedia convergence and power applications, the Company is a major supplier to every industry segment, thanks to its broad range of leading-edge technologies and its rich pool of Intellectual Property (IP) resources.

According to the latest industry data from iSuppli, ST is the world’s fifth largest semiconductor company and is the number one supplier of semiconductors for the Industrial market, application-specific analog chips and power conversion devices. According to In-Stat, ST is the number one supplier for MPEG chips for set-top box applications.  The Company also occupies leading positions in fields as varied as discrete devices, camera modules for mobile phones and automotive integrated circuits, EEPROM memories and the rapidly expanding market for micro-electromechanical systems (MEMS).

Semiconductor products can be broadly divided into two classes: application-specific and multi-segment products. Application-specific products incorporate a significant amount of proprietary IP - from the semiconductor manufacturer, the customer, third parties or any combination of these - that distinguishes them from other products on the market. Examples include:

  • System-on-Chip (SoC) and System-in-Package (SiP) products
  • Custom and semi-custom circuits
  • Application-specific standard products (ASSPs) such as set-top-box chips and automotive ICs 
  • Secure ICs
  • Application Specific Discretes (ASD™).

Once a customer has designed an application-specific product into an application, it is not usually possible to switch to a competitive product without some degree of hardware or software redesign.

In contrast, multi-segment products are devices that perform specific and widely required functions and are usually available from several competing suppliers. Generally, a multi-segment product from one manufacturer can be replaced with an equivalent product from another source and the difference between suppliers tends to be measured primarily in terms of cost and customer service. Once the application design is frozen, however, a multi-segment device can become unique, too, in terms of optimization for maximum performance.

Examples of multi-segment products include:

  • Discrete devices such as transistors, diodes, and thyristors
  •  Power transistors such as MOSFETs, bipolars, and IGBTs
  • Analog circuit building blocks such as op amps, comparators, voltage regulators and references
  • Microcontrollers
  • Standard logic functions and interfaces
  • Stand-alone memory products such as EPROM and EEPROM
  • RF discretes and ICs.

Since its formation, ST has succeeded in balancing its market exposure, combining differentiated application-specific products, which are generally less vulnerable to market cycles, with conventional multi-segment products, which require less R&D effort and manufacturing capital intensity. ST’s diversified product portfolio avoids both an excessively generic approach and an over-dependence on specific applications.

Application-Specific Products
System-on-Chip and System-in-Package Devices
At the most complex end of the application-specific product spectrum are the SoC and SiP devices that integrate a complete system on a single chip or in a multi-chip package. In some cases, this means the integration of the entire application i.e. the resulting device incorporates all of the electronic circuitry apart from components such as displays that are not amenable to integration.  However, integrating the entire system on one chip is not always the most economic solution so the term SoC is also used to refer to chips that integrate a large part of the system.

SoC technology exploits the semiconductor industry’s ability to continually increase the number of transistors that can be integrated in a given silicon area, but it also involves many other factors, including systems knowledge, software expertise, architectural innovation, and design, validation, debug and test methodologies. With the increasing pervasiveness of semiconductor content in electronic devices and its critical impact on the equipment’s performance, price, and development time, equipment manufacturers increasingly rely on semiconductor suppliers to provide complete platform solutions. Today’s platform offerings complement silicon devices with customizable reference designs and full software packages, from low-level drivers and embedded operating systems up to middleware and application software.

Many SoC products can be built using pure CMOS technology but a full SoC capability demands the ability to combine basic functional technologies such as CMOS, bipolar, non-volatile memory, power DMOS, and Micro-Electro-Mechanical System (MEMS) into system-oriented technologies that combine two or more of these basic technologies. For many years ST has been a world leader in developing and deploying these system-oriented technologies.

SoC devices invariably incorporate one or more processor cores and ST offers its customers one of the world’s most impressive ranges of cores, including the 32-bit high-performance ARM- and PowerPC-based products, primarily used in wireless and automotive applications, as well as its Nomadik family of multimedia application processors. ST has an open approach to core technology, with the aim of offering its customers the most appropriate core, whether this is proprietary, jointly developed, or licensed from a third party.

Custom and Semi-Custom Chips
Custom and Semi-Custom ICs are designed and manufactured for one particular customer but they differ in their design and manufacturing methodologies. In a Semi-Custom chip, the starting point is a generic chip containing an array of circuit elements that can be interconnected in various ways to perform desired functions, whereas a Custom chip is designed from scratch. Some customers prefer to design their own chips (especially when the chip incorporates valuable IP) and contract the manufacturing to a chip manufacturer based on criteria such as cost, capacity allocation, and previous business relationships. Others prefer to contract the design as well as the manufacturing to the chip supplier and, of course, there is an entire spectrum of intermediate relationships.

ST offers a full range of Custom and Semi-Custom services that leverage its world-class manufacturing machine, its unrivaled array of semiconductor process technologies, the depth and breadth of its IP portfolio, and its state-of-the-art design methodologies. Among the many successful case histories in ST’s portfolio are the complex chips that power large-scale projects such as digital satellite radio services in the US as well as state-of-the-art solutions provided for strategic partners in every segment of the electronics industry.

Application-Specific Standard Products (ASSPs)
An ASSP (application-specific standard product) is an integrated circuit that is designed for use in a specific application. Examples include, digital set-top box chips, CMOS imaging ICs, motor control circuits and wireless application processors. Unlike a custom IC, which is designed for a specific application of a single customer, an ASSP is designed for a specific application common to many customers. Many ASSPs are developed in close cooperation with particular customers, even though the resulting device may be offered on the open market. By working with customers in this way, ST is able to ensure that the products and technologies it develops closely match evolving industry needs.

ST’s product portfolio includes many types of ASSPs optimized for applications in the key growth segments of Digital Consumer, Computer Peripherals, Automotive and Industrial.  ST is also a key supplier to the Wireless Terminals industry via ST-NXP Wireless, the new company that combines the former wireless businesses of ST and NXP and is a key supplier to leading handset manufacturers including Nokia, Samsung and Sony-Ericsson.

The Company enables its customers to develop and differentiate their products quickly and cost-effectively by supplying its chipsets together with complete reference platforms, proven software packages, and development kits.  This approach has enabled ST to become a world leader in key applications such as Hard Disk Drives, Set-Top Boxes and digital radio.

The Company provides components for a wide array of Digital Consumer applications, with a particular focus on set-top boxes, digital TVs and digital audio, including radio.  In the arena of Computer Peripherals, ST focuses mainly on data storage, printing, visual display units, power management for PC motherboards, and power supplies. A wide range of ST’s ASSPs power sophisticated Automotive systems such as engine control, vehicle safety equipment, door modules, and in-car infotainment  The Company also supplies Industrial ICs for factory automation systems, chips for lighting and battery chargers, or power supply devices, as well as chips for advanced Secure Access applications.

Secure ICs
ST offers a complete range of secure microcontrollers and memory for smartcards and trusted product application segments, together with a broad portfolio of efficient, interoperable System-on-Chip (SoC) solutions. Our products are used in every kind of smart card applications, from the simplest phone cards to the most demanding SIM and Pay-TV cards. Security has always been a special area of expertise for ST, evidenced with a long list of formal security certifications, standardization body memberships, and successful deployments of ST’s Secure IC products in many segments, including Banking, IT Security, e-Government, Public Transport, and Mobile Communications.

Application Specific Discretes (ASD™)
ASD products are based on vertical and horizontal bipolar structures implemented on the top and bottom sides of the silicon wafer substrate. The ASD™ technology has allowed ST to bring to the market numerous products which can handle high bidirectional currents, sustain high voltages, or integrate various discrete elements in a single chip. ASD technology is ideal for general-purpose protection components, ESD protection devices, EMI filters, and AC switches with built-in over-voltage protection. With its recent process upgrade, ASD technology allows the integration, in a single chip, of multiple discrete components and passive elements, such as resistors, capacitors, or inductors, which gave birth to the IPAD (Integrated Passive and Active Devices) family. The main application fields for ASD are wireless and fixed line communications, appliances, PCs, and peripherals.

In-Check “Lab-on-Chip”
ST’s In-Check “lab-on-chip” platform provides integrated genetic analysis at a fraction of the time, cost, and complexity of conventional diagnostic systems. The micro-electro-mechanical solution in a disposable cartridge amplifies tiny DNA samples by precisely controlled heating and cooling cycles and runs biological protocols that evaluate the analyzed substance. ST’s In-Check lab-on-chip opens up new possibilities for real-time and affordable analysis of complex biological substances at the point of need.  The first application, called VereFlu and developed with Veredus Laboratories, detects all major influenza types including the deadly avian influenza H5N1.

Multi-Segment Products
Memories
ST’s non-volatile memory portfolio comprises EPROM (Erasable Programmable Read Only Memory), EEPROM (Electrically Erasable Programmable Read Only Memory), non-volatile RAM (Random Access Memory) and a wide array of RFID ICs. As with all standard devices, cost and customer service are the differentiating factors and ST is fully geared to optimizing these attributes.

Microcontrollers
ST’s microcontroller offering suits every kind of application, from those where minimum cost is the primary requirement to those that need powerful real-time performance and high-level language support. The comprehensive portfolio comprises robust 8-bit general-purpose Flash microcontrollers with standard communication interfaces like USB, CAN, LIN, UART, I²C, and SPI; application-specific 8-bit microcontrollers for applications including brushless motor control, low-noise block converters (LNB), Smart Card readers, USB Flash drives and Programmable System Memories (PSM), which integrate memory functions with a microcontroller and logic on a single chip; 16-bit industry-standard devices and high-performance 32-bit ARM-based Flash microcontrollers with excellent low-power characteristics and advanced connectivity including Ethernet, USB, and CAN.
 
ST’s dedicated microcontroller solutions help accelerate the development of emerging low-data-rate wireless networks, such as Real-Time Location Systems (RTLS) and Zigbee platforms for remote monitoring and control applications.

Smart Power Devices
ST’s smart power devices meet an ever-increasing demand for solutions integrating signal processing parts (analog and/or digital) and power actuators. This design capability offers not only economic advantages but also improvements in terms of reliability, electromagnetic performance, and space and weight reduction. Smart power is a generic term that covers a variety of technologies, lateral as well as vertical, which play important roles to play especially in the automotive market.

VIPower is a family of proprietary ST technologies in which discrete power structure are integrated with analog and digital control and diagnostic circuitry, resulting in a device that combines the robustness of discrete technology with integrated control and diagnostic circuitry. ST’s BCD (Bipolar-CMOS-DMOS) technology combines bipolar, CMOS and DMOS processes, allowing additional system functions, such as voltage regulators, communication interfaces, as well as multiple-load drivers, to be integrated along with logic circuitry in a single device.

Standard Linear and Logic
ST Standard Linear and Logic ICs consist of a broad range of well-known standard devices, as well as many innovative application-specific devices, targeting highly integrated, space-limited applications. The product range includes logic functions, interfaces, operational amplifiers, comparators, low-power audio amplifiers, communication circuits (high-speed analog, infrared, and RF), power-management devices, voltage regulators and references, microprocessor resets and supervisors, analog and digital switches, power switches, VFD drivers, and High Brightness LED drivers.

Discretes
ST is one of the world's leading suppliers of discrete power devices, with a product range that encompasses MOSFETs (including the innovative MDmeshTM second-generation devices), bipolar transistors, IGBTs, Schottky and ultrafast bipolar diodes, triacs, and protection devices. In addition, ST offers a wide range of power modules where multiple power devices such as Schottky diodes, power MOSFETs or IGBTs are assembled in a single package for optimized thermal and reliability performance.

Protection Devices
ST is a long-time world leader in Transient Voltage Suppressors and offers a wide range of solutions, from discrete clamping (TRANSIL™) and crowbar diodes (TRISIL™), to ESD data line protection arrays and protection ICs for telecom circuits.

Sensors
ST is a world leader in MEMS (Micro-Electro-Mechanical Systems) sensors that are able to detect and measure vibration, acceleration, displacement, rotation and inclination in such applications as game systems and mobile terminals and handsets. ST’s MEMS portfolio also includes a range of precision analog and digital temperature sensors that feature lower power consumption and some unique packaging options. The Company also offers highly efficient and flexible touch sensor devices based on capacitive and resistive touch technology to target the growing demand for innovative user interfaces while reducing system cost and increasing reliability.

RF
ST’s RF portfolio includes power RF transistors used in applications such as ISM (Industrial Scientific & Medical), cellular base stations, and two-way portable and mobile radios.

Real-time Clocks
ST offers a complete family of low-power real-time clocks (RTC), ranging from entry-level products to high-end RTCs with microprocessor supervisory functions, SRAM, non-volatile features, and high-level data protection through tamper detect pins. Embedded software calibration permits an accuracy of two seconds per month.

Updated November 2008