| Author | beginning argument ( Replies received: 3 ) |
| yuhao |
Posted 26-11-2008 at 10:01   |

Registered on : 11-26-2009
Messages : 2
OFF-Line
|
Dera all
I met a problem when used I/O port as interrupt.The documentation(RM0016) says STM8S has up to 32 interrupt vectors fixed by hardware,which is the Reference manul for STM8S microcontroller family.And when use STVD , stm8_interrupt_vector.c has 32 interrupt too.But at page 110 in RM0016, interrupt mapping only has 27 interrupt.There are not external interrupt for Port F,G,H,I. If I want to use a pin of Port H to be the interrupt,which registers I should config? And which interrupt vector in vector table in stm8_interrupt_vector.c I should use?
|
|
|
Profile
Quote
|
| bassinux |
Posted 26-11-2008 at 13:08   |

Registered on : 11-15-2009
Messages : 10
OFF-Line
|
Hi Yuhao,
for the STM8S product you can only configure Port A,B,C,D and E, in vector table the Last 4 vectors are not used so not mapped to any peripheral interrupt.
best regards
|
|
|
Profile
Quote
|
| bassinux |
Posted 26-11-2008 at 13:15   |

Registered on : 11-15-2009
Messages : 10
OFF-Line
|
Hi Yuhao,
for the STM8S product you can only configure Port A,B,C,D and E, in vector table the Last 4 vectors are not used so not mapped to any peripheral interrupt.
best regards
|
|
|
Profile
Quote
|
| yuhao |
Posted 27-11-2008 at 15:13   |

Registered on : 11-26-2009
Messages : 2
OFF-Line
|
Hi Bassinux
Thanks very much!
|
|
|
Profile
Quote
|