Device Electronic signature and ID codes
Company  
ST Home | Microcontrollers

Index  »  ARM Cortex-M3 STM32  »  Device Electronic signature and ID codes
     
   Device Electronic signature and ID codes
 Moderated by :   »  STOne-32

Author
beginning argument    ( Replies received: 2 )
ryan.gronlie   Posted 13-11-2008 at 20:57   



Registered on :
10-18-2009

Messages : 17

 OFF-Line

Firstly... I'm curious why the RAM size register has been removed from the latest reference manual (section 25). Can we no longer rely on this register?

Second... I'm having trouble reading the ID code located at 0xE0042000. It works like a charm when I'm executing my code using the debugger. When executing without a debugger all I get back is 0x00000000 (instead of 0x20006410 I get during debugging). Obviously this is a little hard to debug . What am I missing here? I need to enable some register/peripheral to read this when not debugging?



 Profile   Quote  
STOne-32   Posted 14-11-2008 at 16:15   





Registered on :
05-29-2007

From STMicroelectronics

Messages : 455

 OFF-Line

Dear ryan, all,

RAM register size is no more relevant and not existing anymore in our STM32 devices silicon. This is to simplify the software design and to rely only to Flash size which is most important than RAM.

Regarding, the ID code located at 0xE0042000. Refer to STM32 Errata http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110#Errata%20Sheet :

Debug registers cannot be read by user software

The DBGMCU_IDCODE and DBGMCU_CR debug registers are accessible only in debug mode (not accessible by the user software). When these registers are read in user mode, the returned value is 0x00.

Hope this helps you. Cheers,

ST1.




[ This message was edited by: STOne-32 on 14-11-2008 16:15 ]



 Profile   www   Quote  
ryan.gronlie   Posted 19-11-2008 at 00:51   



Registered on :
10-18-2009

Messages : 17

 OFF-Line

Thanks that does explain it.

I really don't understand removing the RAM size register so arbitrarily though.

It doesn't really simplify software design... now I need to do RAM sizing. Before I could just read a register.



 Profile   Quote  
On Top

Search in the forums
 
Jump To