voltage levels of rd,wr,db0-7 on 5v 3433
Company  
ST Home | Microcontrollers

Index  »  µPSD3400  »  voltage levels of rd,wr,db0-7 on 5v 3433
     
   voltage levels of rd,wr,db0-7 on 5v 3433
 Moderated by :   »  uPSD

Author
beginning argument    ( Replies received: 1 )
brigg   Posted 06-11-2008 at 01:22   



Registered on :
08-04-2009

Messages : 1

 OFF-Line

I can not find anywhere that will tell me what the voltage levels of the data buss ale wr and rd signal in a 5 volt system
Can anyone help me



 Profile   Quote  
tim7   Posted 25-11-2008 at 13:18   



Registered on :
11-25-2009

Messages : 2

 OFF-Line

These are MCU signals. The MCU is 3.3V on all models, it is only the PSD that can be 5V. Therefore these are 3.3V levels, ie 0.6V - 2.4V.



 Profile   Quote  
On Top

Search in the forums
 
Jump To