| Author | beginning argument ( Replies received: 2 ) |
| Leogg |
Posted 01-11-2008 at 16:24   |

Registered on : 01-02-2006
From Argentina
Messages : 22
OFF-Line
|
Hi, I have the following issue:
I have two PC for development, both using Rowley's CrossStudio.
My boards have STR711, some with a 4Mhz and some with 14.756 Mhz clock.
On one PC, all boards can be programmed without any trouble.
However, using the second PC I can program the 4 Mhz boards, but not the 14.756 Mhz ones. After first programming failure on these boards, I can't program them anymore, not even in PC1 or PC2, as if the micro was damaged (?). Further programmings results on the same error (please see attached image). Looks like if bytes at offsets 0 goes to offset 8, and bytes at offsets 8 goes to the folowing 0 offset.
It is ver strange. Any tips?
Regards,
Leo
| Attachments : | ErrorJTAG.jpg | | | |
|
|
|
Profile
Quote
|
| Leogg |
Posted 03-11-2008 at 20:06   |

Registered on : 01-02-2006
From Argentina
Messages : 22
OFF-Line
|
Hi,
I made the following test. I took a 14.756 Mhz board, which was already programmed by PC2, so it stopped working. Then, I changed the 14.756 oscillator, placing a 4 Mhz one. Now, it is working again, even in PC2.
So it is an oscillator frequency problem?
I dont quite understand what JTAG requires from board. Or if a user code can disable JTAG interface.
Any tips?
Regards,
Leo
|
|
|
Profile
Quote
|
| myvarmamail |
Posted 11-11-2008 at 10:04   |

Registered on : 11-11-2009
Messages : 1
OFF-Line
|
I am using the wiggler circuit found in net for programming the LPC2106 Micro-Controller though IAR Embedded Workbench for ARM. I am able to download the program into the controller. But unable to set the break points during run time, even though I am setting the break point in advance, the program is not running after coming to that point. If I am trying to enable break point while the controller is running, I am getting a status like “target busy” in the warnings section
| Attachments : | WIGGLER.pdf | | | |
|
|
|
Profile
Quote
|