Difference between single-shunt and three-shunt
Company  
ST Home | Microcontrollers

Index  »  Motor Control  »  Difference between single-shunt and three-shunt
     
   Difference between single-shunt and three-shunt
 Moderated by :   »  tanio  -  arnaudus  -  payet

Author
beginning argument    ( Replies received: 2 )
walterma   Posted 31-10-2008 at 12:59   



Registered on :
09-08-2009

Messages : 8

 OFF-Line

Hi, can you explain what are the advantages and disatvantages of the single-shunt and the three-shunt method for current reading? Thank you!
I've to control a BLDC-Motor with Encoder. What is the best method? Single-Shunt or Three-Shunt???
Thanks!



 Profile   Quote  
gianluigi.forte   Posted 11-11-2008 at 09:16   



Registered on :
01-21-2009

Messages : 18

 OFF-Line

Hi Walterma
the single shunt advantage is the less hardware cost of the solution because it is required only one shunt and one OP amp
the three shunt solution require three shunt and three OP amps.
The reducion of the hardware cost is paid in term of a more complicated algorithm (increase in code size and workload) in term of current distortion (it is required a distortion to allows the current reading) and in term of power dissipation (using the st method)

Best regards
Gigi



 Profile   Quote  
muratterzi   Posted 05-01-2009 at 12:35   



Registered on :
11-03-2009

Messages : 7

 OFF-Line

if you drive motor at low rpm's with a high frequency of load changes , particularly in case you need position control ability first, three-shunt method will be more efficient with respect to controlability.there are some papers about this issue on ieee.it is easy to understand that in case using three shunt resistor, feedback information of motor is multiplied bye 3 in a single revolution. More information gives more good position controlability even at low rpms.


[ This message was edited by: muratterzi on 05-01-2009 12:36 ]


[ This message was edited by: muratterzi on 05-01-2009 12:50 ]







Attachments : decide.gif   
 Profile   Quote  
On Top

Search in the forums
 
Jump To