Psdsoft programming tip required!
Company  
ST Home | Microcontrollers

Index  »  µPSD3300  »  Psdsoft programming tip required!
     
   Psdsoft programming tip required!
 Moderated by :   »  uPSD

Author
beginning argument    ( No reply )
digisys99   Posted 29-10-2008 at 22:26   



Registered on :
10-29-2009

Messages : 2

 OFF-Line

I mapped to use big flash(128K) for data and small one (32K) for code.
As sector is only 8K in secondary flash, how I could declare using PSDsoft?
As my program is bigger than 8K, do I have to declare same hex file for all for sectors in Merging MCU pane???

Thank's!

Here final report...

Memory Start Stop Memory
Block Address Address Data File
--------------------------------------------------------------------------
FS0 [00000 - 07FFF]
FS1 [08000 - 0FFFF]
FS2 [10000 - 17FFF]
FS3 [18000 - 1FFFF]
FS4 [20000 - 27FFF]
FS5 [28000 - 2FFFF]
FS6 [30000 - 37FFF]
FS7 [38000 - 3FFFF]
CSBOOT0[40000 - 41FFF] 0000 1FFF test.hex
CSBOOT1[42000 - 43FFF]
CSBOOT2[44000 - 45FFF]
CSBOOT3[46000 - 47FFF]



 Profile   Quote  
On Top

Search in the forums
 
Jump To