Registered on : 10-09-2009
Messages : 3
OFF-Line
|
Hi,
I modified the Custom_HID USB demo program(STM32) to make it keep sending the data in 'main' function,
int main(void)
{
int i;
unsigned short b;
#ifdef DEBUG
debug();
#endif
Set_System();
USB_Interrupts_Config();
Set_USBClock();
USB_Init();
while (1)
{
for (i = 0; i < 1000000; i++);
b++;
UserToPMABufferCopy((u8 *)&b, GetEPTxAddr(ENDP1), 2);
SetEPTxCount(ENDP1, 2);
SetEPTxValid(ENDP1);
}
}
This firmware works well and the BUSHOUND can get that USB data. I want to make my host program to get that data, I tried to make that program in both Windows and Linux. In Windows, I call SetupDiGetDeviceInterfaceDetail to get the device path of that Custom_HID device, then call CreateFile to open that devicepath. I can properly to get the VID & PID by calling HidD_GetAttributes, but I don't know how to read the data send from Custom_HID device, I tried both HidD_GetFeature, and ReadFile, but failed.
In Linux I used the libusb, after correctly opened that Custom_HID device, I still can not read that data by calling both usb_bulk_read & usb_interrupt_read.
Who can make a sample program to read that data?
Regards,
ZhangZQ
|
|
|