with and without marking A of uPSD3454EB40T6 ? USB affected!
Company  
ST Home | Microcontrollers

Index  »  µPSD3400  »  with and without marking A of uPSD3454EB40T6 ? USB affected!
     
   with and without marking A of uPSD3454EB40T6 ? USB affected!
 Moderated by :   »  uPSD

Author
beginning argument    ( No reply )
Kuni   Posted 21-08-2008 at 12:46   



Registered on :
10-30-2003

From Taiwan

Messages : 139

 OFF-Line

according to the PCN attached, the marking A only related to bond pad re-layout,which should not affect the functionality,
1, however, the USB does perform OK with marking A, but failed in
PC cold boot without marking A! Is the USB function really the same
between these 2 chips!

2, the marking A should be newer since it is new revision, but the attached photos show the one without marking A is newer! Why?










Attachments : DSCF0177.JPG 1166475972.pdf DSCF0178.JPG
 Profile  Email   Quote  
On Top

Search in the forums
 
Jump To