ST10F269 program does not run
Company  
ST Home | Microcontrollers

Index  »  ST10  »  ST10F269 program does not run
     
   ST10F269 program does not run
 Moderated by :   »  Max  -  Kenshin  -  Najoua

Author
beginning argument    ( No reply )
s.jakobeit   Posted 14-08-2008 at 10:54   



Registered on :
08-14-2009

Messages : 1

 OFF-Line

I have built an board with a ST10F269. Im using the port 1L,6,8 as IO and the port 5 as input. I can do a bootstrap over a RS232 connection. The EA-pin is not connected so i think i am in single chip mode. After flashing and making an following reset the programm does not work (run?).
I am using Keil µVision3 for programming.
I have some LEDs on port 1L and I can control them with FlashIt9.

#include "regst10f269.h"
void main(void)
{
DP1L=0xFF;
P1L=0; //LEDs off?
while(1)
{
}
}


[ This message was edited by: s.jakobeit on 14-08-2008 10:55 ]



 Profile   Quote  
On Top

Search in the forums
 
Jump To