Registered on : 04-29-2009
Messages : 4
OFF-Line
|
the code will collapse when I run the below segment in KEIL.I think It's because the cpu frequency is too high,but after i slow down,problem is still. Why? thanks
SCU_AHBPeriphClockConfig(__FMI, ENABLE);
SCU_AHBPeriphReset(__FMI, DISABLE);
FMI_BankRemapConfig(0x4, 0x2, 0x0, 0x80000);
FMI_WriteProtectionCmd(FMI_B1S0, DISABLE);
FMI_EraseSector(FMI_B1S0);
FMI_Timeout_Status = FMI_WaitForLastOperation(FMI_BANK_1); //dead in here
FMI_WriteHalfWord(0x80000,0xAAAA);
FMI_Timeout_Status = FMI_WaitForLastOperation(FMI_BANK_1);
FMI_WriteHalfWord(0x80002,0xAAAA);
FMI_Timeout_Status = FMI_WaitForLastOperation(FMI_BANK_1);
if(FMI_ReadWord(0x80000) == 0xAAAAAAAAUL)
{
LCD_SetCursor(0x42+countof(disp_ln2));
LCD_DISP_CHAR('T');
}
|
|
|