Bit timing issue
Company  
ST Home | Microcontrollers

Index  »  CAN  »  Bit timing issue
     
   Bit timing issue
 Moderated by :   »  Jatin

Author
beginning argument    ( No reply )
j_thakur   Posted 06-06-2008 at 07:25   



Registered on :
03-20-2009

Messages : 4

 OFF-Line

Dear all,
I am using ST72F561R9 controller and the transceiver used is TJA 1050. The crystal used is 16 Mhz. I am able to communicate with 100 kpbs, 125 kbps, 250 kbps and 500 kbps baud rate.

The problem is with the setting of 1 mbps baud rate. i have tried the following settings but unable to get the desired result.
BaudRate CBTR0 CBTR1
1MB 0x01 0x14 / 0x32 / 0x23 / 0x41

Can anobody give the correct setting for the 1 MB baud rate??



 Profile   Quote  
On Top

Search in the forums
 
Jump To