ERASE FLASH
Company  
ST Home | Microcontrollers

Index  »  ST10  »  ERASE FLASH
     
   ERASE FLASH
 Moderated by :   »  Max  -  Kenshin  -  Najoua

Author
beginning argument    ( Replies received: 2 )
newsamo   Posted 29-05-2008 at 13:58   



Registered on :
10-15-2009

Messages : 14

 OFF-Line

I'm working on st10f168 with st10flasher, now, load monitor is ok, dump is ok, but i'm not able to program flash because appears error messagea boute flash erase: EraseFlash failed.flash

How can i erase ?



 Profile   Quote  
Najoua   Posted 02-06-2008 at 10:35   





Registered on :
12-22-2003

From Tunisia

Messages : 305

 OFF-Line

Hello Newsamo,

Programming voltage (12V) of the on-chip Flash memory must be supplied to pin VPP(pin 84).

Is the 12V ensured in this pin during programming/erasing operation?
Best regards,
Najoua.



 Profile   Quote  
joluci   Posted 18-09-2008 at 05:54   



Registered on :
03-28-2009

Messages : 1

 OFF-Line

Hello Najoua,

in which others microcontrollers of st10fxxx family I need to apply the voltage programming to erase and program?

Thank you !!!



 Profile   Quote  
On Top

Search in the forums
 
Jump To