reading bad internal SRAM data
Company  
ST Home | Microcontrollers

Index  »  µPSD3300  »  reading bad internal SRAM data
     
   reading bad internal SRAM data
 Moderated by :   »  uPSD

Author
beginning argument    ( Replies received: 1 )
aa   Posted 27-03-2008 at 22:20   



Registered on :
03-27-2009

Messages : 3

 OFF-Line

Hello,

I use a UPSD3354DV-40u6 and have a problem with reading the internal SRAM.

After testing several pcb boards the result is that I have boards that read
corrupt data from the internal SRAM. After debugging I have seen that a wrong board
has a "bad signal" at the databus when reading at an adres in SRAM. With "bad signal" I
mean that it is not a nice "1" but a slow rising signal from "0" to "1" like loading a capacitor.
Other external busdrivers can drive the bus and are tri-state at the moment the SRAM is reading.

(seen with a scoop that triggerd on the \RD pin an looking at MCUAD0 (multiplexed databus 0)).


After some testing the board is working fine and it have a good signal.

Please let me know if you have some tips or suggestions to solve this problem.

Best regards,

André



 Profile   Quote  
aa   Posted 28-03-2008 at 20:13   



Registered on :
03-27-2009

Messages : 3

 OFF-Line

Hello all,

The problem is solved. The reasen was that the battery voltage (PC2) was sometime above the Vdd so thhe SRAM goes in protection mode.

Best regards,

André



 Profile   Quote  
On Top

Search in the forums
 
Jump To