| Author | beginning argument ( Replies received: 1 ) |
| basvandijk86 |
Posted 23-11-2007 at 12:23   |

Registered on : 11-23-2009
Messages : 8
OFF-Line
|
Hi, I am normally using the NXP LPC2129 but for a project I need 2 controllers so I want to use the ST73x .. I am the Hitex STR730 (by Keil) evaluation board.
And an the Insiders Guide, first it all looks the same as the NXP (also ARM7) but I saw that I can only use the functions already written, I cannot write the registers and let it work (like the NXP). So it's all really confusing me at the moment.
I really would like to use CAN0 and CAN1, they must have an receive interrupts and if there is an interrupt they must read the received data.
Also it must be possible to write their own data to CAN but I just can't get it working. Does anyone has some kind of example code or any hints.
I found some but those are so complicated and big. I did code this for the NPX in about 20 lines.. it cannot be that the ST need like 500 lines isn't it?
Hope someone can help me out.
|
|
|
Profile
Quote
|
| c.wesseling |
Posted 08-04-2008 at 18:05   |

Registered on : 02-12-2009
Messages : 2
OFF-Line
|
does someone have an easy2use sample up to now? - same problme as above....
[ This message was edited by: c.wesseling on 08-04-2008 18:06 ]
|
|
|
Profile
Quote
|