Code and Data in the CSBOOT memory
Company  
ST Home | Microcontrollers

Index  »  µPSD3400  »  Code and Data in the CSBOOT memory
     
   Code and Data in the CSBOOT memory
 Moderated by :   »  uPSD

Author
beginning argument    ( Replies received: 1 )
sagam   Posted 12-11-2007 at 16:12   



Registered on :
11-12-2009

Messages : 1

 OFF-Line

I'm using the 3454 wit the main memory used as data and CSBOOT0-2 as code, and CSBOOT3 as programmable data page (in PSDExpress the sec. memory is defined as code&data - so the VM is good). Everything is working just fine but when I try to erase sector CSBOOT3 to write new data to it, the MCU will 'freeze' until reset. The CSBOOT3 is set to page 8 and mapped to 0x8000-0x9FFF as it should be. Writing to any sector of the main flash (using the same code different pages)works just fine. Can someone help and explain what I'm doing wrong, or point to a similar code example (code and data within the CSBOOT memory)? Thanks!



 Profile   Quote  
phaze426   Posted 03-01-2008 at 15:51   



Registered on :
10-08-2003

From USA

Messages : 156

 OFF-Line

sagam,

The flash memory banks in the uPSD are not write-while-execute capable. What this means is that if you're running code in CSBOOTX, you cannot at the same time program/erase ANY other CSBOOT area. You'll have to be running from RAM or from FSX (main flash) if you want to reprogram the CSBOOT sectors. This is the reason there are these two separate areas in the chip.

-Phaze426



 Profile  Email   Quote  
On Top

Search in the forums
 
Jump To