Read 25P10AV
Company  
ST Home | Microcontrollers

Index  »  ST5  »  Read 25P10AV
     
   Read 25P10AV
 Moderated by :   »  Nino

Author
beginning argument    ( Replies received: 1 )
mr_spokk   Posted 19-09-2007 at 21:30   



Registered on :
09-19-2007

From Sweden

Messages : 1

 OFF-Line

Hi, I just wonder if there is any simple soulution to read out the bin-file from that chip?
The Pcb board that I have is not functional and I need to read out the info from the 25P10AV.
I have a SOIC Clip from Pomona to put the wirings on, is there any simple way to connect it to the Com or Lpt port?
If so what program do you recommend to use for reading the chip?

Best Regards

Bosse


[ This message was edited by: mr_spokk on 19-09-2007 21:31 ]



 Profile   Quote  
Nino   Posted 20-09-2007 at 09:35   





Registered on :
10-01-2002

Messages : 33

 OFF-Line

Hi,

may be you are in the wrong forum. ST52 is an 8bit microcontroller.

Best Regards



 Profile   Quote  
On Top

Search in the forums
 
Jump To