Need an example application for ST52F513
Company  
ST Home | Microcontrollers

Index  »  ST5  »  Need an example application for ST52F513
     
   Need an example application for ST52F513
 Moderated by :   »  Nino

Author
beginning argument    ( Replies received: 4 )
Spkt   Posted 02-05-2006 at 23:59   



Registered on :
04-23-2006

From 0

Messages : 9

 OFF-Line

Hi all,
Can someone post up an example application designed for ST52F513?
Thanks!


[ This message was edited by: Spkt on 03-05-2006 00:00 ]



 Profile   Quote  
Nino   Posted 03-05-2006 at 14:38   





Registered on :
10-01-2002

Messages : 33

 OFF-Line

If you mean a schematic example, please see in the attachment.




Attachments : example_sch.pdf   
 Profile   Quote  
Spkt   Posted 03-05-2006 at 23:13   



Registered on :
04-23-2006

From 0

Messages : 9

 OFF-Line

Hi Nino,
Thanks for the schematics, but I actually need a code (a .fs4 project file). You know my problem about the chip not working when put in the circuit from the other tread. I want to program the chip with the example code to see if it works this time. This way I can decide if the problem is with my own code or the way I set up the chip in circuit.



[ This message was edited by: Spkt on 03-05-2006 23:14 ]



 Profile   Quote  
Nino   Posted 05-05-2006 at 15:56   





Registered on :
10-01-2002

Messages : 33

 OFF-Line

OK. Try with this example: it is a simple use of the AD and the SCI (without any sense, to be simple to read).




Attachments : example.FS4   
 Profile   Quote  
Spkt   Posted 06-05-2006 at 23:57   



Registered on :
04-23-2006

From 0

Messages : 9

 OFF-Line

Hi Nino,
I can't tell if the chip is working with the example you provided. I only have a multimeter at home, and I don't know which pins to measure to see if the chip is running as it is supposed to. Do you have an example that brings certain pins high and low with a delay/ or puts out a measurable PWM wave for me to check?
Thanx!



 Profile   Quote  
On Top

Search in the forums
 
Jump To