external ram in upsd33xx
Company  
ST Home | Microcontrollers

Index  »  µPSD3200  »  external ram in upsd33xx
     
   external ram in upsd33xx
 Moderated by :   »  uPSD

Author
beginning argument    ( Replies received: 2 )
siksik   Posted 07-01-2004 at 11:14   



Registered on :
01-07-2004

From Israel

Messages : 2

 OFF-Line

Hi,
I want to connect an external ram to a upsd3333 using the pld for latching the address. i used the PA port for the low address bus.
1. Where should i connect the data-bus? to AD[0..7] or to a port?
2. Do i have to use the ALE signal? Can i leave it unconnected?
3. I need a RAM with 17 bit address. Can i use PB port for the high bits
of the address-bus :A[12..16]?
4.Do you have an application-note with a shema of a upsd3333 with
an external RAM?
Thanks,


 Profile   www   Quote  
uPSD   Posted 08-01-2004 at 00:31   





Registered on :
12-10-2002

Messages : 281

 OFF-Line

1. D7-D0 of external RAM should be connected to AD7-AD0 on the uPSD.
2. You can configure port A as "Latched Address Out", and connect PA7-PA0 to A7-A0 of the external RAM. Please see the attached picture. Connect mcu A11 - mcu A8 to ext. RAM A11-A8.
3. uPSD is 8032 based, a standard 8032 only has 16-bit address bus and can address up to 64K memory when memory paging is NOT used. To address beyond 64K, memory paging must be used. You can use PB3-PB0 and write PLD equations like the example shown in AN1560 (a15_x - a12_x) and connect them to A15 - A12 of your ext. RAM.
4. Sorry we do not have an app. note on this subject.



Attachments : XRAM_addr.bmp   
 Profile   Quote  
khtang   Posted 08-05-2008 at 08:38   



Registered on :
05-02-2009

Messages : 1

 OFF-Line

I am using uPSD3422 and I tried to map the PA and PB ports to latched address low and lateched address high as described without success. I do not get any expected address out.

My solution is to define these pins as Combinational logic output, then at the Design Assistant's I/O Logic Equation page I equate these pins to the corresponding adresses, i.e. pa7 = a7, pb7 = a15, etc. I also tie the Output enable pins of these pins to _reset. It seems to work.

Any idea or comment to my solution?

[ This message was edited by: khtang on 08-05-2008 08:40 ]



 Profile   Quote  
On Top

Search in the forums
 
Jump To