| Author | beginning argument ( Replies received: 1 ) |
| marcel.sigrist |
Posted 29-04-2008 at 17:11   |

Registered on : 04-29-2008
Messages : 1
OFF-Line
|
Last week my ULINK1 USB-JTAG Connector was broken.
Today I received a new ULINK2. But the new ULINK2 doesn't work.
When I tried to programming my uPSD3354DV chip following error occurred:
Erasing Flash...
Erasing PLD/ACR...
Programming Flash Block 0 (FS0)
Flash Programming Error in Block: 0x00000 - 0x00039
***Error: Programming failed
The firmware version of the ULINK2 is V1.30.
The Softwareversion of Keil uVision is V3.60.
For the Flash Programming I use the St -uPSD ULINK Driver. (UL2UPSD.DLL
V2.63)
With another ULINK2 (Print Version 1) I bought last year I can download a program without problems to the uPSD3354.
I already tried a second ULINK2 (Print Version 2) because i believed the first ULINK2 was broken. But both ULINK2 doesn't work.
Do you have any suggestions for solving the problem?
|
|
|
Profile
Quote
|
| info41 |
Posted 17-06-2008 at 19:33   |

Registered on : 06-17-2008
Messages : 1
OFF-Line
|
Dear Marcel,
I had the same errors in the past. I think i collected all the possible errors from ULINK2 and PSD Soft.
I don't know exactly the possible cause but i played around the MERGE FILE SECTION of PSD Soft Express and the phenomena disappeared.
For me something is related with HEX file addressing. I moved and changed the related .H0x files and finally i found a stable configuration.
Take a look inside your HEX files (I suppose you have several) and check if these files have the right addresses for the Flash area you configured.
Luca
|
|
|
Profile
Quote
|